This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEMU110-U: Can XDS110 (TMDSEMU110-U) supports HSM debugging?

Part Number: TMDSEMU110-U

Whether the XDS110 having TI Part# TMDSEMU110-U is able to handle HSM debugging or not? if HSM debugging needs to be done, is this XDS110 sufficient or should  we buy the new device?

  • Yes, this tool can be used for HSM debugging as well,

    HSM core is like any other core on the device, It is connected to the debug subsystem like other CPU cores, so any debugger able to debug application cores, wil support HSM core deugging as well.