Part Number: AM2612
Hi TI experts,
When integrating the LBIST function based on SDK mcu_plus_sdk_am261x_11_00_00_28 in SBL, the initialization of STL under the APP caused the program to crash. The STL version is AM261x_STL_10_02_00_02, and STL only has the Lib library but no source code.May I ask if you have encountered a similar situation?
Best Regards
Bruvin