Part Number: TDA4APE-Q1
Hi experts,
We are developing a custom board based on TDA4APE. The system is equipped with multiple 12M cameras. Therefore we have high requirements for image encoding and decoding capabilities.
According to the chip manual, the maximum image encoding capability is 960 MP/s. However, in actual test, we used the GStreamer tool to encode four streams simultaneously at 25 fps with a 12M camera, and no issues were encountered. The corresponding theoretical encoding capability is 12 × 25 × 4 = 1200 MP/s, which exceeds the specifications in the chip manual.

Is the encoding capability described in the manual accurate? Or is there an issue with our test method?
This affects our software solution selection, so please help confirm this.
Best Regards.