Part Number: AM2434
Hello,
I'm currently running into weird problems while accessing the DMSC via the SCI client. My current guess for the root cause is that I'm overriding the already existing firewall configuration for MSRAMK7. While debugging I have realized that there are already a bunch of configurations set, right after the null bootloader. I assume they are required for the DMSC, as the DMSC uses a part of MSRAMK7? Which of those region configurations are necessary, because almost all of the 8 regions are already preconfigured? I'm asking because there would be space in MSRAMK7 left, which is unused by DMSC. But without available firewall regions unfortunately I won't be able to utilize this memory range.
Kind regards,
Benedikt Schmidt