This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224: The value after reset for several FLASH registers not as documented

Part Number: TMS570LS1224

a) Flash Pump Access Control Register 1 (FPAC1) 

The register description states the value after reset for the PSLEEP field bits 26-16 is 64h, however during development I am seeing C8h

b) EEPROM Emulation ECC Register (FEMU_ECC)

The register description states the value after reset for the EMU_ECC[7:0] field bits 7-0 is 3h, however during development I am seeing 0h

c) Flash Bank Fallback Power Register (FBFALLBACK) 

The register description states the value after reset for reserved bits 31-16 is 0505h, however during development I am seeing 0000h

d) Flash Bank Configuration Register (FCFG_BANK)

The register description states the value after reset for reserved bits 3-0 is 2h, however during development I am seeing 1h