Part Number: TMDSCNCD263P
Other Parts Discussed in Thread: SYSCONFIG
Hi,
I recently posted on this topic regarding failures of the MMC/SD examples on a LP-AM263Px. This is in addition to a large post regarding failure of etherent examples, which was fixed with a patch from TI.
We purchased new hardware and still have the same failures. We have tested multiple SD cards with different file system formats and different partition options, none work.
All examples appear to ID the card correctly, but fail after switching to 4bit mode.
The output from the test we get is:
[Cortex_R5_0] [MMCSD FILE IO] Starting...
Some tests have failed!!
Our SDK is mcu_plus_sdk_am263px_11_01_00_19 and the example in question on this board is mmcsd_file_io_am263px-cc_r5fss0-0_freertos_ti-arm-clang, however all other examples we have tested, including the raw examples fail in the same way.
Hopefully someone from TI can shed some light on why the tests fail, and maybe even confirm if there is an issue in the driver code when switching to 4 bit mode.
Thanks.