Part Number: AM263P4-Q1
Other Parts Discussed in Thread: SYSCONFIG
When RPMessage_send() is called five times in a row with a timeout of 0 ms, the following warning is output and SystemP_TIMEOUT is returned.
"RPMessage_send:288: [IPC RPMSG] Message send to remote core 3 @ 2 end point failed due to lack of space in Notify Queue!!!"
Please tell me the cause and solution.
Even when called 16 times in a row, this warning is output only the fifth time, and not from the sixth time onwards.
The "RP Message Number of Buffers" setting in sysconfig is 16.
Also, the warning is not output when the timeout is set to 1 ms.
There is sufficient vring, and the following warning is output when the vring queue overflows, so I believe this is a different cause.
"[IPC RPMSG] Message send to remote core %d @ %d end point failed due to lack of space in vring!!!"