Part Number: MSPM0C1105
Can the MSPM0C1105 microcontroller has the BSL enabled by default, so that it can be invoked via hardware pins, without needing to reprogram the NONMAIN flash?
We are designing a product that includes muliple microcontrollers that are connected by UART. It will not be practical for us to program all of them by jTag during production, so we want to use the ROM BSL to program them oser the UART. We have done this with other TI MSPM microcontrollers using the NRST and BOOT pins. The slau893c datasheet indicates that BOOTCFG2 BOOTMODE defaults to 0xFFFF which means the BSL is disabled.
Are there any part variants or other ways of achievening this using this part?