Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65261-1: Circuit design issues based on the TPS65261

Part Number: TPS65261-1
Other Parts Discussed in Thread: TPS65261

Dear Technical Support Team

We are currently using the TPS65261_1RHBR in our project to generate 1.1V, 1.5V, and 2.5V. When measuring the power‑up time of the 2.5V and 1.5V rails, we observed a voltage bump on the waveform, as shown in the red box in the figure.

I would like to understand the cause of this voltage bump. In addition, since this bump generally occurs within 500 mV, I would like to know whether it may have any negative impact on the system. If optimization is required, what aspects should be adjusted to reduce or eliminate this voltage bump? Thank you.

image.png

image.png