Part Number: AM2432
Hi,
I am using AM2432 with the Industrial SDK 11.00.00.08.
I am interested in using DKEK to encrypt data.
I'm reading here that there are two possible mechanisms, but I've had problems with both. Using the first mechanism to provide the DKEK directly to SA2UL, I couldn't find where to set the USE_DKEK in SA2UL security context flag. But in both cases, when I try to use the functions declared here, the compiler always reports "unresolved symbol Sciclient_set/get/releaseDKEK".
Is the use of DKEK actually supported on the AM2432? Is there a step I'm missing? Is there a example that uses it?
Thank you,
Best Regards,
Andrea