This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM13E23019: Questions about AM13E2x I2C driverlib

Part Number: AM13E23019

While working with I2C peripheral using driverlib module from am13e2x SDK version 01.00.00.EA2, we had some findings about the following:

  • DL_I2CC_DMA_INTERRUPT_TXFIFO_TRIGGER
    This definition mapped to non-existent UNICOMMI2CC_DMA_TRIG1_IMASK_TXTRG_SET. It seems that it should be UNICOMMI2CC_DMA_TRIG0_IMASK_TXTRG_SET.

  • DL_I2CC_enableDMAEvent
    This function accepts DL_I2CC_EVENT_ROUTE and DL_I2CC_DMA_INTERRUPT, which we found hard to untangle.
    This isn't a bug or a problem for us, but rather the feedback that we spent some time connecting all the ends:
    In the SDK, routes are enumerated as 1 and 2 and fixed to DMA_TRIG1 and DMA_TRIG0 accordingly, while in the TRM, they are not explicitly enumerated. At the same time, each DMA_TRIGx has its own IMASK register (also not explicitly tightened in the TRM description) that serves a specific purpose -- TX or RX irq.
    For the SW developers, it would be nice to, perhaps, improve naming (e.g. route_tx, instead of route_rx) or relationship descriptions in the TRM and/or have some mapping in the driverlib for easier work

  • DL_I2CC_getRXFIFOCounter/DL_I2CC_getTXFIFOCounter
    1. These functions are supposed to return the number of bytes that can be read from FIFO, but returns value of SR_BCNT, which seems to serve a different purpose
    2. In DL_I2CC_getRXFIFOCounter, the value is not shifted by UNICOMMI2CC_SR_BCNT_OFS

BR,
Oleksandr

  • Hi Oleksandr,

    DL_I2CC_DMA_INTERRUPT_TXFIFO_TRIGGER
    This definition mapped to non-existent UNICOMMI2CC_DMA_TRIG1_IMASK_TXTRG_SET. It seems that it should be UNICOMMI2CC_DMA_TRIG0_IMASK_TXTRG_SET.

    This has been fixed in the SDK that was released in mid-march. The v26.00.00.06 version has the reference 

    DL_I2CC_enableDMAEvent
    This function accepts DL_I2CC_EVENT_ROUTE and DL_I2CC_DMA_INTERRUPT, which we found hard to untangle.
    This isn't a bug or a problem for us, but rather the feedback that we spent some time connecting all the ends:
    In the SDK, routes are enumerated as 1 and 2 and fixed to DMA_TRIG1 and DMA_TRIG0 accordingly, while in the TRM, they are not explicitly enumerated. At the same time, each DMA_TRIGx has its own IMASK register (also not explicitly tightened in the TRM description) that serves a specific purpose -- TX or RX irq.
    For the SW developers, it would be nice to, perhaps, improve naming (e.g. route_tx, instead of route_rx) or relationship descriptions in the TRM and/or have some mapping in the driverlib for easier work

    I'll share this feedback with both the software and the production applications team.

    DL_I2CC_getRXFIFOCounter/DL_I2CC_getTXFIFOCounter
    1. These functions are supposed to return the number of bytes that can be read from FIFO, but returns value of SR_BCNT, which seems to serve a different purpose

    The BCNT is actually the max data that can be read from the RxFIFO or TxFIFO in the Controller, before starting a transaction we set the BCNT value as an indication of " how many bytes this transaction is going to last for ", so it makes sense to return the BCNT in this design.

    2. In DL_I2CC_getRXFIFOCounter, the value is not shifted by UNICOMMI2CC_SR_BCNT_OFS

    This looks like a valid bug, i've reported it internally and this should be taken care in the next SDK release (Internal tracking link: https://jira.itg.ti.com/browse/MSDK-1788)

    Regards,
    Shaunak

  • Hello Shaunak, thank you for the response!

    • This has been fixed in the SDK that was released in mid-march. The v26.00.00.06 version has the reference
    • The latest version I can find is 01.00.00.EA2 from Feb 18. Maybe you can share the reference where we can get it, please?
    • Screenshot you attached still maps DL_I2CC_DMA_INTERRUPT_TXFIFO_TRIGGER to UNICOMMI2CC_DMA_TRIG1_IMASK_TXTRG_SET, which seems to be wrong. From the TRM, we would expect mapping to TRIG0, or have we misread the TRM?
    • Thank you very much!
    • The BCNT is actually the max data that can be read from the RxFIFO or TxFIFO in the Controller, before starting a transaction we set the BCNT value as an indication of " how many bytes this transaction is going to last for ", so it makes sense to return the BCNT in this design
    • Ok, thank you, I think we've missed that SR.BCNT is updated by hardware when the transfer length is > 1.
    • This looks like a valid bug, i've reported it internally and this should be taken care in the next SDK release (Internal tracking link: jira.itg.ti.com/.../MSDK-1788)

    • What will be your suggestion on how to proceed with the current thread (e.g. keep it open until your internal ticket is resolved)?

BR,
Oleksandr

  • Another concern about BCNT:

    It holds up to 0xFFF bytes and, in my understanding, represents the total length of the transfer, which can be higher than the max FIFO size (16 bytes).

    So if we have a 20-byte-long message to send, at first, TX will be filled with 16 bytes of data, and BCNT will be loaded with 20, which does not correspond to the actual FIFO level

  • Hi Oleksandr,

    You can find the latest SDK at: https://www.ti.com/tool/download/AM13E2X-SDK

    Updated product page: https://www.ti.com/product/AM13E23019

    In future, all the latest SDKs and TRMs will be uploaded directly to the product page and the SDK pages

    Regarding the I2C Bug, i'll keep this thread open until the bug is fixed and i can provide a patch.

    Also, i checked in the driver, the I2C DMA integration is not yet complete. The design I see right now is that the I2CT (target) is mapped to DMA_TRIG0 and I2CC (controller) is mapped to DMA_TRG1. This design can change if it has issues when the DMA support gets integrated, which is currently scoped in for 26.01 release (mid june).

    Also, for the question regarding BCNT:

    The BCNT will be loaded with 20 bytes, and only when the 20 bytes are processed a STOP condition would be issued. Once data is loaded into the FIFO, the count would be reduced from BCNT, so after FIFO is filled with 16 bytes, BCNT will become 4, and so on, once the 4 bytes are filled, BCNT will become 0, and a stop will be triggered.

  • Hi Shaunak!

    About the IRQ triggers. We followed the next logic from TRM (which works in our driver implementation):

    The second publisher(DL_I2CC_EVENT_ROUTE_1) is tied to TRIG 1 and the third(DL_I2CC_EVENT_ROUTE_2) to TRIG0:

    From the TRM table 25-20. "UNICOMMI2CT_REGS Registers" we see that interrupt-related registers have 3 groups, where we expect 2nd group to correspond to TRIG1 and 3rd to TRIG0:

    3rd group (offset 88h) corresponds to TXTRG flag:

    From this we conclude that:

    TX trigger <-> TRIG0 <-> 3rd publisher <-> DL_I2CC_EVENT_ROUTE_2

    RX trigger <-> TRIG1 <-> 2nd publisher <-> DL_I2CC_EVENT_ROUTE_1

    *This configuration worked in our tests

     

    Additionally, in the SDK v26.00.00.06 I see that DL_I2CC_DMA_INTERRUPT_TXFIFO_TRIGGER/DL_I2CC_DMA_INTERRUPT_RXFIFO_TRIGGER are the same as in the 01.00.00.EA2:

    1. DL_I2CC_DMA_INTERRUPT_TXFIFO_TRIGGER mapped to UNICOMMI2CC_DMA_TRIG1_IMASK_TXTRG_SET, while UNICOMMI2CC_DMA_TRIG1_IMASK_TXTRG_SET do not exist

    2. DL_I2CC_DMA_INTERRUPT_TXFIFO_TRIGGER and DL_I2CC_DMA_INTERRUPT_RXFIFO_TRIGGER are mapped to the same TRIG1, which seems impossible according to TRM.

    I'm not sure that the design you mentioned will work, as RX and TX must have separate routes to trigger separate DMA channels, so they cannot be both tied to one TRIG, or have I misunderstood the architecture?

    ----------------------------------------------------------------------------------

    About BCNT:

    Yes, exactly. And this means that BCNT does not contain the "number of bytes which can be read from RX FIFO"/"number of bytes which can be put into TX FIFO" as the SDK documents for functions DL_I2CC_getRXFIFOCounter/DL_I2CC_getTXFIFOCounter. To me, this sounds like these functions do not behave like they are supposed to. At the same time, I don't see any possible replacement for BCNT (e.g. MSPM0G had separate FIFO status registers for this purpose).

    For now, this is not a blocker for us, but we would like you to clarify the behaviour of these functions and improve documentation/remove them if functionality is not achievable

    BR,
    Oleksandr

  • Hi Oleksandr,

    Yes I agree with the comment on DL_I2CC_DMA_INTERRUPT_TXFIFO_TRIGGER. It has been remapped to UNICOMMI2CC_DMA_TRIG0_IMASK_TXTRG_SET in the internal SDK, the last public SDK released has this bug.

    Your analysis is correct.

    Regarding the BCNT, unlike MSPM0 we dont have a FIFO status register which will give exact count of data in the Tx/Rx FIFO, we can just check if there is Data in FIFO/FIFO is empty. One way to go around would be to subtract the value returned by BCNT from a known value that is configured for transaction count. For example, in this case, if 20B is configured and after 16B of transfer, you read back the BCNT as 4B, then handle the calculation as "20-4" to get FIFO count. This is a bit hacky but since we lack the register like MSPM0, this is one way to implement the FIFO read function. I agree the comments in the function need to be modified.

    Let me share this feedback with the SDK to either rename/remove/reword the API.

    Regards,
    Shaunak

  • Thank you, Shaunak!

    We will wait for the updates regarding fixes from you.

    BR,
    Oleksandr