Part Number: AM2434
We are in the process of designing a automotive test tool using the AM2434 processor. In a previous version of this product we had a TI 5409A DSP that generated a 12 MHz clock for the FPGA (on BCLKR0). In the new design we would like to generate a similar clock from the AM2434 processor, but does not have to be exactly 12 MHz. It looks like OBSCLK0 or MCU_OBSCL0 might be able to generate such a clock. However, the Reference Manual states that these outputs are for observation purposes to be used for test and debug. Is there any reason why we cannot used one of these to generate our FPGA clock during normal system operation?