This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294NCPDT: TM4C1294NCPDT : ROM boot loader

Part Number: TM4C1294NCPDT

Hello,

According to SPMU301E (TivaWare™ Boot Loader ), if the entire TIVA flash is erased (e.g address 0x0000.0004 ), 

then boot loader runs and enables to update application. 

Am I right ?

In this case, should I expect any ouput on the serial interface ?

If there is no application that initiate the UART, how this is possible ?

Thank you,

Zvi