Part Number: AM2612
Champs:
My cust asked those questions, please reply for each.
1. How is the single code can achieve ASIL-B / SIL2? Any example / document to address this?
2. If the code working success rate is 100%, so, the safety is 100%, this has no problem. But, if the code will be fail somehow, so the sucess rate is 0%, why the fail rate can be 7x% or 9x%? Plz explain.
3. Is there any SIL-3 function safety code for BMS regarding the OTP/OCP/OVP? Any documentation?
4. The Pbist.c only shows the printf, how to determine my code is having the safety score is 90% and map this score into the FMEDA table?
How the FMEDA table can judge my code's success rate?
How the FMEDA table knows my code is safety score with 95% ? not 0%?
5. After my studying, there is 3rd party tool can evluate my code success rate, what's the recommened tool?
Thanks.
BR Rio