Part Number: TMS320F280039C
Other Parts Discussed in Thread: LP-XDS110,
Hello,
I have recently purchased an LP-XDS110 to program and debug the TMS320F280039C. I am currently designing a custom board and would like to confirm the correct implementation and software setup.
1. Hardware Connection: My custom board uses a 1.27mm pitch cTI 20-pin header. Since the LP-XDS110 has a 2.54mm pitch output, I understand that a pitch conversion is necessary.
-
Does the LP-XDS110 fully support the 5-pin JTAG (including nTRST) required for C2000 devices via its 20-pin header?
-
Are there any specific pinout requirements for the 1.27mm cTI 20-pin header to ensure compatibility with the LP-XDS110? (e.g., specific wiring for EMU0/EMU1 or nTRST on pin 19).
2. Software Configuration (CCS):
-
What is the recommended "Connection" setting in the Code Composer Studio (CCS)
.ccxmlfile for the LP-XDS110? -
Are there any known issues or specific TCLK frequency settings I should be aware of when using LP-XDS110 with the F280039C?
I would appreciate it if you could verify if this setup is officially supported and if there are any technical notes for this specific combination.
Best regards,
Nam Hoon, Kim