Part Number: MSPM0G5187
I'm working with a customer planning to use the MSPM0G5187 device for its NPU AI accelerator capability. The design does not have USB in it. They will be utilizing the Standby0 or Standby1 mode, and want to ensure lowest possible current consumption in these modes.
It is unclear from the documentation what the hardware configuration of the VUSB33 pin should be when the USB feature is unused. Should it be:
- Unconnected?
- Pulled up or down?
- Connected to VDD (nominal 3.3V)?
- Something else?
Thanks,
Stuart