Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G1518: input impedance of the comparator

Part Number: MSPM0G1518

Hello team, 

What is the value of the input impedance of the comparator? As this parameter does not appear to be explicitly specified in the datasheet 

Thank you!

  • Hi Diana,

    The input of COMP is Hi-Z, can you help me understand why users care about this spec?

    Internally within the MCU, the pins are shared between the GPIO and the COMP; normally the impedance of the GPIO is significantly [edit, fix a typo, smaller] larger than that of the COMP.

    Based on the leakage current at the I/O port, the overall impedance is estimated to exceed 66 MΩ:

    B.R.

    Sal

  • Hi Sal, 

    Thank you for the reply. 

    The customer wants to use the MCU-integrated comparator for the charger C 6C-22 and therefore needs the input impedance of this comparator.

    Best regards,

    Diana