Part Number: MSPM0L1228
hi ,
from datasheet, I can only see leakage for below.

how about the leakage current of HDIO and ODIO on MSPM0L1228?
BR,
frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSPM0L1228
hi ,
from datasheet, I can only see leakage for below.

how about the leakage current of HDIO and ODIO on MSPM0L1228?
BR,
frank
Hi Sal,
This is Phison AE Wills.
I would like to clarify whether the HDIO, DOIO, and SDIO leakage current specifications in the datasheet are applicable only at VDD = 3.3 V.
Thank you.
Hi Wills,
When VDD = 0 V, do these IOs have the same leakage limits, or are there separate specifications for the unpowered state?
The leakage current is the spec when VSS<=VIN<=VDD in a certain IO.
(Or maybe: VSS-0.3<VIN<VDD+0.3, I am not sure which one is the MSP standard)

I think if the VDD=0V, users shoud take care on VIN of the IO pins.
As for leakge current, I think it follow the same spec under the recommended / absolute max ratings.
B.R.
Sal
Are the leakage current specifications for HDIO, DOIO, and SDIO defined only for the powered condition (for example, VDD = 3.3 V as stated in the datasheet)?
Hi Wills,
Within recommendation range, the IO leakage current should have same limitation:

With the range of 0V<VDD<1.62V, I am not sure whether it also applied the same max limitation, as internal circuit might not work.
If VDD=0, the MCU impedance has no meanings, as your input to the IO pin should also be 0V. Then no leakage current is expected.
B.R.
Sal