This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2432: Co existence of CPSW and PRU-ICSS ethernet

Part Number: AM2432

Hello team,

 

My customer implemeted CPSW based 2 ports ethernet and EtherCAT slave based on PRU-ICSS on AM2432 and each projects worked well on lanchpad. but when they combined these 2 projects into one, PRU-ICSS based EtherCAT worked well and CPSW, 1 port worked well but the other one didn't worked well.

ETHPHY1 worked well and ETHPHY0 didn't worked well.

 

if customer wants to use those all 4 ports, what should be checked?

 

Regards,

Ted

  • Hi Ted,

    Can you please let us know the platform being used for testing the final integration of the application?

    Which MII mode are CPSW and ICSS configured in? I am assuming the customer is using EtherCAT with ICSS-M. Am I correct? If not, please confirm if the customer is using ICSS-G or ICSS-M. 

    Thanks and regards,
    Teja.