Part Number: MSPM0G3519-Q1
Hello TI team,
we are using MCAL_MSPM0_00.02.05.00 and found several constants/variables that are mapped to wrong MemMap section:
Cdd_I2c_Cfg.c:
CONST(uint32,CDD_I2C_CONST)CddI2cHwUnitBaseAddr[CDD_I2C_HW_UNITS_MAX] is a const, but mapped to VAR_INIT_32 section.
Can_Cfg.c:
const struct Can_ControllerStruct_PC *CanConfigSet_CanController_List_PC[CAN_NUM_CONTROLLER] is a const, but mapped to CFG_DATA_INIT.
const struct Can_MailboxStruct_PC *CanConfigSet_CanHardwareObject_List_PC[CAN_NUM_MAILBOXES] is a const, but mapped to CFG_DATA_INIT.
Can_Mcan.c:
static const uint8 Can_McanDataSize[16] = {0U, 1U, 2U, 3U,
is a const, but mapped to VAR_INIT_8.
are const, but mapped to VAR_INIT_32.