Part Number: MSPM0C1103
Other Parts Discussed in Thread: MSPM0C1104, , UNIFLASH
As far as I understand from the reference manual that factory reset is supported for these two devices MSPM0C1103 and MSPM0C1104.
I tried to perform "Factory Reset Auto" from Uniflash on both devices and it was not performed successfully. I don't have any issues regarding connection to the target. I can normally re-flash and read memory but factory reset is not possible. Please check the log where Uniflash hangs after instead of applying factory reset successfully.
Is this a bug in Uniflash? or is the reference manual contains wrong information that maybe both devices don't support factory reset besides that they don't also support mass erase?
What alternative i can use to perform factory reset if Uniflash is buggy? I followed this thread
to execute factory reset manually using dslite scripts but it is not easy to modify all required files correctly to get the correct commands to perform factory reset for these specific small devices.
I would appreciate any help regarding this matter!