CCSTUDIO-THEIA: CCSTUDIO V20.3.1.5 is not starting on Ubuntu 22.04

Part Number: CCSTUDIO-THEIA

Hello Ti experts,
Currently I'm working on TI's AM62P5-SK board. And for MCU and DM core side development using FreeRTOS I'm using TI's CCS(Code Composer Studio) Version 20.3.1.5: Link

Earlier it was starting when given start command for CCS, but suddenly from last week the CCS is taking more time to start around 2-3 hours. For reference I've attached 10 seconds video of what I'm seeing when executing binary.


Even I'm having enough disk space + RAM.

aditya@VETC-DW-73G3R24:~$ free -h
               total        used        free      shared  buff/cache   available
Mem:           125Gi       7.0Gi       105Gi       264Mi        12Gi       117Gi
Swap:          2.0Gi          0B       2.0Gi
aditya@VETC-DW-73G3R24:~$ df -h
Filesystem      Size  Used Avail Use% Mounted on
tmpfs            13G  3.2M   13G   1% /run
/dev/nvme1n1p2  468G  164G  281G  37% /
tmpfs            63G  2.7M   63G   1% /dev/shm
tmpfs           5.0M  4.0K  5.0M   1% /run/lock
efivarfs        432K  278K  150K  65% /sys/firmware/efi/efivars
/dev/nvme0n1p1  511M   72M  440M  14% /boot/efi
tmpfs            13G  1.7M   13G   1% /run/user/1000
aditya@VETC-DW-73G3R24:~$ 

Due to failure in start of CCS our development speed is slowered, Kindly provide support on this as soon as possible.

Regards,
Aditya T