Part Number: AM2432
Other Parts Discussed in Thread: SYSCONFIG
Hi,
I am using AM2432 with the Industrial SDK 11.00.00.08.
Our various projects involve the use of the industrial protocols Profinet, Ethernet/IP, and IEC 61850, as well as CPSW.
Due to supply issues with LPDDR4, we are exploring alternatives. I read here (under 3.3 LPDDR4 Interface Schematics) that the AM243x only supports DDR in single-channel mode. Is it still possible to use DDR dual-channel by forcing the single-channel option (for example, by not connecting the second channel that is not supported)?
Are there any specific consequences we should expect that would be worth investigating? Especially in relation to the specific details of the industrial protocols we are adopting.
Alternatively, do you see any problems in principle with using only MSRAM and Flash with XIP mode for the various protocols we use? I’ve seen that, in theory, the Profinet and Ethernet/IP demos are also compatible with the Launchpad, which doesn’t have DDR, so I don’t expect any particular issues.
Thank you,
Best Regards,
Andrea