Part Number: MSPM0L2228
Hello,
What direction is the -2 mA on the I_d spec here:

Does -2 mA mean 2 mA INTO the MSPM0? Or out of the MSPM0?
Munan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSPM0L2228
Hello,
What direction is the -2 mA on the I_d spec here:

Does -2 mA mean 2 mA INTO the MSPM0? Or out of the MSPM0?
Munan
Hi Munan,
The negative value should mean that the current is flowing out of the pin.
Thanks!
Hey Morgan,
Thanks for the feedback, why is the positive current into the diode so low? This is way lower than most of the other MSPM0's
Munan
Hey Munan,
That device uses a special type of IO. The high side injection current was very limited which is why you see it being lower than other M0's.
-Morgan