This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM13E23019: Wrong ECC address calculation in DriverLib

Part Number: AM13E23019

When using SDK version 01.00.00.EA2 (26.00.00.06 seems to have the same problem), we faced unexpected failures when trying to erase the sector, receiving DL_FLASH_COMMAND_FAIL_BLANK_VERIFY error. We believe this is caused by the wrong ECC address calculation in the function DL_FlashCTL_blankVerify from the dl_flashctl module of DriverLib.

Function DL_FlashCTL_blankVerify calculates the ECC address for the given flash word by dividing its address by 16. From our observation, this looks up the ECC for the wrong flash word.

According to the AM13E230x TRM (MARCH 2026 revision), e.g., "ECC code address returns the 16-bit ECC value for the entire 128-bit flash word that was accessed."(10.1.2.3.1 Flash Memory Map), the flash word size is 16 bytes(128bits) and the corresponding ECC is 2 bytes (16 bits), so we expect this scaling factor to be 16(128)/2(16) = 8.

For our tests, we've already applied this scaling factor as a workaround and confirmed the correct behaviour of the application.

Could you please confirm our assumption about this bug in the SDK, and if so, inform us when the fix is expected?

BR,
Oleksandr