Part Number: TMDSEMU200-U
Other Parts Discussed in Thread: TMDS64EVM, CCSTUDIO, UNIFLASH, TMDSEMU110-U
Hi Team,
I am using TMDS64EVM with external debugger TMDSEMU200-U connected to J25.
Previously the same setup was working, but now CCS cannot communicate with the XDS200.
CCS error:
Texas Instruments XDS2xx USB Debug Probe_0/CS_DAP_0 Error initializing emulator:
(Error -2083 @ 0x0) Unable to communicate with the debug probe.
Confirm debug probe configuration and connections, reset the debug probe,
and retry the operation. (Emulation package 20.4.0.3835)
Test Connection from .ccxml advance settings gives:
-----[Print the board config pathname(s)]------------------------------------
C:\Users\SOURAV~1.SIN\AppData\Local\TEXASI~1\
CCS\ccs2040\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_io
Failed to open i/o connection (xds2xxu:0)
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.
I also tried XDS200 firmware recovery/update using:
C:\ti\ccs2040\ccs\ccs_base\common\uscif\xds2xx>update_xds2xx.bat xds200
Output:
Updating Firmware ...
Rebooting, please wait ...
Updating CPLD ...
Reading Configuration ...
boardRev=2
ipAddress=0.0.0.0
ipConfig=dhcp
ipGateway=255.255.255.255
ipNetmask=255.255.255.255
productClass=XDS2XX
productName=XDS200
serialNum=S200-000FD2068290
swRev=1.0.0.9
hostCPU=AM1802
emuCtrlType=Bit bang
extMemType=SDRAM
portUSB=true
portENET=false
portWIFI=false
portRS232=false
EnableUSBSerial=true
CurrentMeasure=false
So firmware update succeeds and PC detects the XDS200, but CCS still cannot connect.
How can I fix this issue?
Thanks.