This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263PX-MCAL-SDK: SDL example

Part Number: AM263PX-MCAL-SDK
Other Parts Discussed in Thread: LP-AM263P

Hi,

I am using an LP-AM263P board, CCS 20.5.1, SDK 26_00_00_06.

I have built the mcan_sdl_am263px-cc_r5fss0-0_freertos_ti-arm-clang example.

The board is programmed with the pre-built sbl_ospi_multicore_elf boot code and the mcelf from the SDL example build.

However on reset I see the boot loader output but nothing from the application.

Starting OSPI Bootloader ... 
KPI_DATA: [BOOTLOADER_PROFILE] CPU Clock        : 400.000 MHz 
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media       : NOR SPI FLASH 
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media Clock : 133.333 MHz 
KPI_DATA: [BOOTLOADER_PROFILE] Boot Image Size  : 86 KB 
KPI_DATA: [BOOTLOADER_PROFILE] Cores present    : 
r5f0-0
KPI_DATA: [BOOTLOADER PROFILE] System_init                      :        517us 
KPI_DATA: [BOOTLOADER PROFILE] Drivers_open                     :        102us 
KPI_DATA: [BOOTLOADER PROFILE] LoadHsmRtFw                      :      10346us 
KPI_DATA: [BOOTLOADER PROFILE] Board_driversOpen                :       2341us 
KPI_DATA: [BOOTLOADER PROFILE] CPU load                         :       4925us 
KPI_DATA: [BOOTLOADER PROFILE] SBL End                          :          5us 
KPI_DATA: [BOOTLOADER_PROFILE] SBL Total Time Taken             :      18237us 

Image loading done, switching to application ...

Is there some step I am missing?

Regards

Neil