This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1117: Does MSPM0L1117 Support Mutli-Word Programming?

Part Number: MSPM0L1117

I see enum DL_FLASHCTL_COMMAND_SIZE below in the flash driver but I do not see any write routies for sizes greater than one word (64-bit).  If I try to write data to FLASHCTL.CMDDATA2 (0x400ce138) it will not take but no error is asserted.  I assume this means multi-word programming is not supported however, I can not explicitly find this statement in any documentation (datasheet or reference manual).

/*! @enum DL_FLASHCTL_COMMAND_SIZE */
typedef enum {
    /*! Flash Command size is one word */
    DL_FLASHCTL_COMMAND_SIZE_ONE_WORD = FLASHCTL_CMDTYPE_SIZE_ONEWORD,
    /*! Flash Command size is two words */
    DL_FLASHCTL_COMMAND_SIZE_TWO_WORDS = FLASHCTL_CMDTYPE_SIZE_TWOWORD,
    /*! Flash Command size is four words */
    DL_FLASHCTL_COMMAND_SIZE_FOUR_WORDS = FLASHCTL_CMDTYPE_SIZE_FOURWORD,
    /*! Flash Command size is eight words */
    DL_FLASHCTL_COMMAND_SIZE_EIGHT_WORDS = FLASHCTL_CMDTYPE_SIZE_EIGHTWORD,
    /*! Flash Command size is a sector */
    DL_FLASHCTL_COMMAND_SIZE_SECTOR = FLASHCTL_CMDTYPE_SIZE_SECTOR,
    /*! Flash Command size is a bank */
    DL_FLASHCTL_COMMAND_SIZE_BANK = FLASHCTL_CMDTYPE_SIZE_BANK

} DL_FLASHCTL_COMMAND_SIZE;