Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG
All of the ethernet based SDK examples for the AM2434 are based on the R5-0-0 core. However, in my application I have all 4 R5 cores almost fully utilized. Is it feasible/possible to port one of these working examples to the M4 core to take on all the Lwip heavy lifting?
If it matters, I've started from the SDK 12.0.0.26 example called
mcu_plus_sdk_am243x_12_00_00_26\source\networking\enet\core\examples\lwip\enet_cpsw_udp_igmp\am243x-lp
and I'm working to adapt that example to only allow ping and unicast udp tx, which so far is working well, albeit on the wrong core. My hope was to be able to optimize it down to only use the resources that it needs for my application and then port it over to the M4 core of my project.
From the perspective of sysconfig it would seem that operating ethernet on the M4 is not possible, but perhaps I can at least get the M4 to manage the heavy lifting and just have the R5-0-0 core manage a light DMA ISR trigger as needed.
I should also note that I have a DMA channel almost fully utilized on to make block data transfers between a PRU and the R5-0-0, so hopefully operating this ethernet Lwip driver won't cause conflicts or performance issues with that.
Should I have hope or am I taking a wrong turn?
Thanks,
Marshall