Part Number: CC3220SF
I2CCC32XX_MAX_BURST is defined in source/ti/drivers/i2c/I2CCC32XX.c with a value of 255.
/* Determine the size of this burst */
if (object->readCount > I2CCC32XX_MAX_BURST)
{
object->burstCount = I2CCC32XX_MAX_BURST;
}
else
{
object->burstCount = object->readCount;
}
The value of burst count is later validated via an assert with a condition that does not match:
void
I2CMasterBurstLengthSet(uint32_t ui32Base, uint8_t ui8Length)
{
//
// Check the arguments.
//
ASSERT(_I2CBaseValid(ui32Base) && (ui8Length < 255));
//
// Set the burst length.
//
HWREG(ui32Base + I2C_O_MBLEN) = ui8Length;
}
The assert is triggered when trying to read >254 bytes. Should I2CCC32XX_MAX_BURST be set to 254 or the assert condition removed (since the data type already limits the value to range 0-255)?
SDK version 7.10.00.13.