Other Parts Discussed in Thread: TMS570LS20216, HALCOGEN
hi again,
Im using the TMS570LS20216
when I use the CanTransmit () function I see the TrReqX and TrReq34 (mailbox=33) are set according to the mailbox number,
same is for NewDatX and NewDat34. (I configured the external loopback test mode).
then I am trying to read using the canGetData() function, and it clears NewDatX and NewDat34 but the TrReqX and TrReq34 are still set.
because the TrReqX and TrReq34 not cleared I cannt transmit once again to the same mailbox (33).
Do TrReqX and TrReq34 should be cleared to transmit again to same mailbox? if yes, what clears it?
One more Question: During the transmition I use an osciloscope to check the CANH and CANL pins (I have the USB Stick EV),
but I see nothing although I used the External loopback. why?
thanks alot
Gil