This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VIC code in HALCoGen for TMS570?

Hi,

I was looking at the sys_startup.c file for the TMS570 as generated by HALCoGen and noticed a call to this function:

_coreEnableIrqVicOffset_

mrc p15, #0, r0, c1, c0, #0
orr r0, r0, #0x01000000
mcr p15, #0, r0, c1, c0, #0
bx lr

.endasmfunc

Seeing as there is no VIC on the TMS570, is this an unnecessary init function or is there something going on here that the function naming does not represent?

Thanks,
Marco
  • Marco,

    Document SPNU499 on page 610 (15.2.3 Software Interrupt Handling Options) describes the 3 different mode of operation for the VIM.
    Option 3 Hardware vectored interrupt behavior must be explicitly enabled by setting the vector enable (VE) bit in the CP15 R1 register.

    This is the purpose of  the _coreEnableIrqVicOffset_ routine.

    Please let me know if I've answered your question.

    Thanks and Regards,

    Jean-Marc