This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM261: BiSS-C not work properly

Part Number: LP-AM261
Other Parts Discussed in Thread: BP-AM2BLDCSERVO, TIDA-010979

Hi Experts,

We tried BiSS-C example project 'bissc_diagnostic_single_channel_am261x-lp_r5fss0-0_freertos_ti-arm-clang' imported from motor_control_sdk_am261x_2025_00_00_01 SDK on LP-AM261 Rev.A + BP-AM2BLDCSERVO EVMs + Eyou actuator(the one in TIDA-010979).

We can build up source code and run successfully as below uart message where our encoder used is 19-bit resolution without multi-turn (MPN is iC-MU150). One thing weird is that there is always singleturn angel output with CRC failure at the both cases of attaching and de-attaching encoder.

 

Could you please help check and provide any suggestion? Thanks in advance.

 

<UART message>

BiSS-C firmware         : 1.1.6 (release)


|------------------------------------------------------------------------------|
 BiSS-C Instance 0
 PRU-ICSS instance: 1, PRU-ICSS slice number: 0

BiSS-C Single channel, Single PRU Demo application is running......

Channel 0 is enabled

=======================================================================
                                                                       BiSS-C Frame Size Constraints:
                                                                                                       - Without Safety: single_turn + multi_turn <= 56 b
its
     - With Safety: single_turn + multi_turn <= 40 bits
                                                       =======================================================================

Please enter encoder lengths connected to Channel 0:

Please enter 1st encoder single turn length
                                           19

Please enter 1st encoder multiturn length, 0 if not multiturn
                                                             0

Please enter 0 as data length if daisy chain is not used

Please enter 2nd encoder single turn length
                                           0

|------------------------------------------------------------------------------|


 PRU-ICSS firmware loading is complete

BiSS-C encoder/encoders detected and running at frequency 1 MHz for BiSS-C instance 0

Processing Delay in clock cycles for BiSS-C instance 0 channel 0 : 1

|------------------------------------------------------------------------------|
|                             Select input parameters                          |                                                                         
|------------------------------------------------------------------------------|
| 1 : Number of position data bits                                             |
| 2 : Select clock frequency in MHz(1/2/5/8/10)                                |
| 3 : Encoder send position values                                             |
| 4 : Control Communication - Register Read/Write                              |
| 5 : Loop over BiSS-C cycles                                                  |
| 6 : Start periodic continuous mode (CMP trigger)                             |
| 7 : Start periodic continuous mode (CAP trigger)                             |
| 8 : Enable safety mode                                                       |
| 9 : Configure encoder timeout                                                |
| 0 : Exit the application                                                     |
|------------------------------------------------------------------------------|
| Enter value:
3

 BiSS-C instance 0:

 Channel 0:

 Encoder-1 Singleturn Angle:  36.851577759000, crc:0x7, otf crc:0x12, e_w:0x0

 CRC Status: failure, crc error count: 1

|------------------------------------------------------------------------------|
|                             Select input parameters                          |
|------------------------------------------------------------------------------|
| 1 : Number of position data bits                                             |
| 2 : Select clock frequency in MHz(1/2/5/8/10)                                |
| 3 : Encoder send position values                                             |
| 4 : Control Communication - Register Read/Write                              |
| 5 : Loop over BiSS-C cycles                                                  |
| 6 : Start periodic continuous mode (CMP trigger)                             |
| 7 : Start periodic continuous mode (CAP trigger)                             |
| 8 : Enable safety mode                                                       |
| 9 : Configure encoder timeout                                                |
| 0 : Exit the application                                                     |
|------------------------------------------------------------------------------|
| Enter value:
3

 BiSS-C instance 0:

 ERROR: Position data measurement timeout for BiSS-C instance 0

 Channel 0:

 Encoder-1 Singleturn Angle:  36.851577759000, crc:0x7, otf crc:0x12, e_w:0x0

 CRC Status: failure, crc error count: 1

|------------------------------------------------------------------------------|
|                             Select input parameters                          |
|------------------------------------------------------------------------------|
| 1 : Number of position data bits                                             |
| 2 : Select clock frequency in MHz(1/2/5/8/10)                                |
| 3 : Encoder send position values                                             |
| 4 : Control Communication - Register Read/Write                              |
| 5 : Loop over BiSS-C cycles                                                  |
| 6 : Start periodic continuous mode (CMP trigger)                             |
| 7 : Start periodic continuous mode (CAP trigger)                             |
| 8 : Enable safety mode                                                       |
| 9 : Configure encoder timeout                                                |
| 0 : Exit the application                                                     |
|------------------------------------------------------------------------------|
| Enter value: