Part Number: AM2612
Other Parts Discussed in Thread: TMS320F28388D, UNIFLASH
Hi,
Could you check below questions?
For dual-core products, is it possible to share peripherals between cores?
(For example, if Core1 uses UART1 and Core2 uses UART2, can each core observe the other's peripheral? Can they access each other's RAM?)
Customer has been using TMS320F28388D. In the AM series, is there a mandatory master core that must operate, or are the cores equivalent without a main core designation?
Regarding PRU-ICSS: Should this be considered as a separate core dedicated to communication apart from the dual cores? Can stack firmware be downloaded via debugger or UniFlash?
Looking at the AM261x as an example, PRU-ICSS appears to be an independent core that should be connected to the 3-port Ethernet function. Is this configuration user-definable?
When downloading the stack to PRU-ICSS, is there a separate flash memory area independent from the flash on the main cores? (Checking where the stack is downloaded)
Thanks.