Part Number: AM2612
Hello team,
what is the maximum data size that a single channel PRU can handle in a BISS encoder input?
Are 48 bits of data supported?
Best regards
Manuel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2612
Hello team,
what is the maximum data size that a single channel PRU can handle in a BISS encoder input?
Are 48 bits of data supported?
Best regards
Manuel
Manuel
Our solution can support 48 bits without safety mode enabled. Following are the constraints (also documented in application available in SDK):
Regards
Dhaval
Hello Dhaval,
thank you for the reply.
Can you please also tell me how long the PRU needs to start the next cycle when it is triggered at 16kHz?
Best regards
Manuel
Manuel
It depends on BiSS-C frequency, encoder resolution and encoder timeout.
Time taken for one position read is determined by the frequency and resolution. After encoder sends position, there is typically a timeout as defined in BiSS-C specification, during which we can not trigger a new position read. Timeout for a specific encoder can be found out from it's datasheet.
Regards
Dhaval