This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2612: PET for Multicore use cases

Part Number: AM2612

Dear Experts,

I am planning to use AM261x.

To take care on the core utilization, I would like to understand how we should handle if the cores are acting as dual coare with different utilization.

Fore example: 

Core 1 is running at 70%

Core 2 is runnign at 30% utilization

How to consider this in ower Power Estimation tool

image.png

According to the note shown above, this would be: 
50% *0.3 +50%*0.7 
or will we need to consider worst case 70%? 

Regards,
Alex