Part Number: AM263P4-Q1
Other Parts Discussed in Thread: AM263P4,
Hi team,
For the part AM263P4 ,please share the asssembly soldring or refloew profile
Regards
Jayakeerthana P
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM263P4-Q1
Other Parts Discussed in Thread: AM263P4,
Hi team,
For the part AM263P4 ,please share the asssembly soldring or refloew profile
Regards
Jayakeerthana P
Please correct it to assembly soldering or reflow profile
Hi Jayakeerthana,
The AM263P4-Q1 uses an NFBGA (ZCZ) 324-pin package with a moisture sensitivity level of MSL Level-3-260C-168 HR [1]. This means:
For PCB guidance specific to the AM263x family (refer to the AM263x Hardware Design Guide, Section on PCB Assembly [2].
| Parameter | Specification |
|---|---|
| Peak temperature | 260°C max |
| Time above 217°C (liquidus) | 60–150 seconds |
| Ramp-up rate | 3°C/s max |
| Preheat/soak | 150–200°C for 60–120 seconds |
| Peak time (within 5°C of peak) | 20–40 seconds |
| Ramp-down rate | 6°C/s max |

(Excerpt from: AN-1126 BGA (Ball Grid Array) (Rev. C))
Since this is an MSL-3 device, if the dry-pack seal is broken for more than 168 hours, baking is required before reflow (typically 24 hours at 125°C per J-STD-033).
Best Regards,
Zackary Fleenor