Part Number: AM263P4-Q1
AM263Px MCU+SDK (mcu_plus_sdk_am263px_10_01_00_31) SBL (OSPI): Question about linker.cmd memory map intent
I would like to confirm the intent of the memory map in the linker script for the AM263Px MCU+SDK SBL (OSPI). I am referencing the following file:
...\examples\drivers\boot\sbl_ospi\am263px-lp\r5fss0-0_nortos\ti-arm-clang\generated\linker.cmd
Q1: MSRAM_VECS start address 0x70002000
In the linker script, MSRAM_VECS starts at 0x70002000.
Can the address range 0x70000000–0x70001FFF (the first 8KB) be used by the SBL?
If this region is reserved, what is it used for?
Q2: Reducing MSRAM_HSMRT size
From my side, it looks like MSRAM_HSMRT actual usage is only about ~26KB.
Is it safe to reduce the allocated size of MSRAM_HSMRT? If there is a minimum required size or any constraint, could you please advise?
Requested response date: June 19, 2026