This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: How to use MDIV of G3507

Part Number: MSPM0G3507
Other Parts Discussed in Thread: ENERGYTRACE,

Hi,

I would like to set CPUCLK to 1MHz.
According to technical reference manual, when user want to set less than 4MHz, it seems that we can use MDIV.
So, I set MDIV following caution of technical reference manual, I can see less than 4MHz signal but I see something strenge point. So could you please confirm about below ?

 Q1 : When I set 2MHz setting, I could see following signal (observe this signal by enabling CLK_OUT function.)
image.png
Actually, frequency is 2MHz but duty ratio is strange (For clock, in my understanding, duty ratio should be 1:1.)
Is it expected result ?

Q2 : 
When I set 1MHz setting, I could NOT see 1MHz signal. (same signal as 2MHz pattern.)
Is it expected result ?

Best Regards,