This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Failed connect to the xds100 emulator with IAR kickstart



Hello, 

I'm evaluating both CCS and IAR to develop with the Hercules RM48 MCU,

I have a development kit, the CCS worked fine,

but I was not able to download to the target ( using XDS 100 ) from IAR,

I got the message :

------------------

Thu Feb 16, 2012 21:26:59: Fatal error: Failed to connect to the xds100 emulator (connect DAP)... 
 (Error -600 @ 0x0) A required dynamic library could not be located. 
The library isn't on the search path. 
(Release 0.0.0.0)     
Session aborted! 

---------------

I've tried to change the search path

project options -> Debugger ->TI XDS 100 

in the field "TI emulation package installation path"

no success,

anyone has any idea or a example project in IAR with the right config to XDS 100 ?

thanks,

Cristiano