Part Number: TMDSEMU200-U
Dear TI Support Team,
I am experiencing a communication issue with two TMDSEMU200-U (XDS200) debug probes, both of which are under warranty.
The probes are unable to maintain a stable USB connection with Windows. When connected, they appear briefly in Device Manager and then disconnect after a few seconds, preventing reliable communication with the target device.
I was able to verify that the firmware is already updated and functioning correctly. Since the issue is present on both units and persists across different USB ports and systems, I suspect a hardware-related problem rather than a firmware issue.
Could you please advise on the recommended troubleshooting steps and the warranty replacement/RMA process for these units?
Thank you for your assistance.
Best regards,
Sachin