This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3351: u-boot 2026.04 defconfig Build Issues

Part Number: AM3351

Using the U-Boot 2026.04 release, I built a MLO file based on the am335x_evm_defconfig file.

Redoing the u-boot build using the 2017 Linux 4.9 product baseline ‘devel_am335x_defconfig’ file, the build fails with various ‘make’ pre-script check errors.

Reviewing the 2017 Linux 4.9 product baseline ‘devel_am335x_defconfig’ file, I also found missing ‘oMap’ configuration statements.

Need TI help in addressing the 2017 Linux 4.9 product baseline ‘devel_am335x_defconfig’ file u-boot build issues.

I see two paths forward to resolve the u-boot build issues:

  1. Modify the U-Boot 2026.04 release am335x_evm_defconfig file --
  • Using u-boot menuconfig, modify the ‘am335’ configuration statements for our product hardware.
  1. Modify the 2017 Linux 4.9 product baseline ‘devel_am335x_defconfig’ file --
  • Add the missing ‘oMap’ configuration statements.
  • Resolve the 2026.04 MLO build issues by updating the defconfig file.

 

 

  • Hi ,

    The owner is on leave today; he will address this once back,
    Thanks,
    JOMY
  • Hi Bob,

    Before the assigned engineer looking into your query, can you please clarify on what you are trying to do with both u-boot 2026.04 and 2017 sdk u-boot? I am a bit confused by your description. It seems you are trying to use the u-boot defconfig from 2017 to build 2026.04, is this correct?

    Regardless the u-boot version, it already provides configs/am335x_evm_defconfig. You'd better to use it as the baseline but please do not take the defconfig file across u-boot versions.

    Please also note, for latest u-boot, the TI officially supported version is 2026.01, not 2026.04 and any other 2026 versions.

  • >>> It seems you are trying to use u-boot defconfig file from 2017 u-boot?????

    The best path forward is the following:

    1. Modify the U-Boot 2026.04 release am335x_evm_defconfig file -- (Best Path Forward, in my view.)
    • Using u-boot menuconfig, modify the ‘am335x’ configuration statements for our product hardware. (If Required.)

     

    >>> ‘Target’ firmware build environment??

    Our ‘Target’ firmware built under ‘Buildroot’ open source project.  (Linux Mint 20.)

    ‘U-boot’ built under u-boot ‘config’ and ‘build’ make commands. (Linux Mint 20.)

     

    >>> Cross-Compile Tools used to build u-boot ??

    Installed GCC 10 (gcc 10.5) version:

        sudo apt-get install gcc-10 g++-10

        gcc-10 --version

        g++-10 --version

     

    Installed the GCC 10.3 ARM Cross-Compiler package version:

      gcc-arm-10.3-2021.07-x86_64-arm-none-linux-gnueabihf.tar.xz

     

     

    Questions for TI:

    1. The TI SDK supported version of u-boot is 01. Is this correct??
    2. Should I download the TI SDK ‘Tools’ package ‘PROCESSOR-SDK-LINUX-AM335X’ from ti.com/tool/download support site??? Is the SDK Tools package required to build u-boot or apply patches to u-boot source??
    3. Should I download the TI supported version of u-boot 01 from ‘DasBoot’ GitHub site??
    4. The ‘New’ 01 u-boot will load and startup Linux version 4.9. Do you expect any startup issues or problems that must be addressed??
    5. What modifications do I have to make to the ‘am335x_evm_defconfig’ file for Linux version 9 OS startup??
  • Hi Bob,

    • The TI SDK supported version of u-boot is 01. Is this correct??
    • Should I download the TI SDK ‘Tools’ package ‘PROCESSOR-SDK-LINUX-AM335X’ from ti.com/tool/download support site??? Is the SDK Tools package required to build u-boot or apply patches to u-boot source??
    • Should I download the TI supported version of u-boot 01 from ‘DasBoot’ GitHub site??
    • The ‘New’ 01 u-boot will load and startup Linux version 4.9. Do you expect any startup issues or problems that must be addressed??
    • What modifications do I have to make to the ‘am335x_evm_defconfig’ file for Linux version 9 OS startup??
    1. Yes, 2025.01 (2026.01, as part of SDK v12 is not yet released for AM335x)
    2. You can either download the TI Processor SDK Linux, or set it up using Yocto. (https://www.ti.com/tool/PROCESSOR-SDK-AM335X#downloads)
      The Processor SDK bundles pre-tested patches, defconfigs, and cross-compilers aligned to the SoC
    3. If you need to download it separately, (it will be downloaded along with the SDK) - TI's U-boot fork is recommented
      https://github.com/TexasInstruments/ti-u-boot
    4.  There may be DT/bootargs compatibility concerns. 4.9 is very old. TI hasn't tested this combination, so we recommend to test carefully.
    5. Mostly boot command env vars (bootargs, fdtfile, bootcmd) — the Kconfig symbols themselves don't usually change for kernel version.

    Regards,
    Vinu

  • Hi Bob,

    We have tried U-boot 2025.01(from SDK 11.2) with Kernel 4.19 (from SDK 6) and got it booting.

    Steps:

    1. Created SD card using SDK 11 create-sdcard.sh script. (Boot partition size was small in SDK 6)
    2. Replaced zImage and am335x-boneblack.dtb in the boot partition with kernel and dtb from SDK 6 prebuilt images.
    3. Replaced rootfs partition contents of the SD card with SDK 6 rootfs (tisdk-rootfs-image-am335x-evm.tar.xz).
    4. Updated extlinux.conf with the following


    # Generic Distro Configuration file generated by OpenEmbedded
    LABEL Arago
        KERNEL ../zImage
        FDT ../am335x-boneblack.dtb
        APPEND root=PARTUUID=${uuid} rootwait rw earlycon console=${console},${baudrate}

    PFA bootlogs

    U-Boot SPL 2025.01-00718-ga44465cad8a3 (Nov 14 2025 - 10:48:56 +0000)
    Trying to boot from MMC1
    
    
    U-Boot 2025.01-00718-ga44465cad8a3 (Nov 14 2025 - 10:48:56 +0000)
    
    CPU  : AM335X-GP rev 2.1
    Model: TI AM335x BeagleBone Black
    DRAM:  512 MiB
    Core:  162 devices, 19 uclasses, devicetree: separate
    WDT:   Started wdt@44e35000 with servicing every 1000ms (60s timeout)
    NAND:  0 MiB
    MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
    Loading Environment from FAT... Unable to read "uboot.env" from mmc0:1... 
    <ethaddr> not set. Validating first E-fuse MAC
    Net:   eth2: ethernet@4a100000using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
    MAC de:ad:be:ef:00:01
    HOST MAC de:ad:be:ef:00:00
    RNDIS ready
    , eth3: usb_ether
    Hit any key to stop autoboot:  0 
    switch to partitions #0, OK
    mmc0 is current device
    Scanning mmc 0:1...
    Found /extlinux/extlinux.conf
    Retrieving file: /extlinux/extlinux.conf
    1:	Arago
    Retrieving file: /extlinux/../zImage
    append: root=PARTUUID=19afe4c8-02 rootwait rw earlycon console=ttyO0,115200n8,115200
    Retrieving file: /extlinux/../am335x-boneblack.dtb
    Kernel image @ 0x82000000 [ 0x000000 - 0x415200 ]
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
    Working FDT set to 88000000
       Loading Device Tree to 8fff4000, end 8fffff6c ... OK
    Working FDT set to 8fff4000
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Linux version 4.19.94-gbe5389fd85 (oe-user@oe-host) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 PREEMPT Sun Apr 19 03:43:09 UTC 2020
    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [    0.000000] OF: fdt: Machine model: TI AM335x BeagleBone Black
    [    0.000000] earlycon: omap8250 at MMIO 0x44e09000 (options '')
    [    0.000000] bootconsole [omap8250] enabled
    [    0.000000] Memory policy: Data cache writeback
    [    0.000000] efi: Getting EFI parameters from FDT:
    [    0.000000] efi: UEFI not found.
    [    0.000000] cma: Reserved 48 MiB at 0x9d000000
    [    0.000000] CPU: All CPU(s) started in SVC mode.
    [    0.000000] AM335X ES2.1 (sgx neon)
    [    0.000000] random: get_random_bytes called from start_kernel+0xa4/0x434 with crng_init=0
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 129920
    [    0.000000] Kernel command line: root=PARTUUID=19afe4c8-02 rootwait rw earlycon console=ttyO0,115200n8,115200
    [    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Memory: 455952K/524288K available (9216K kernel code, 307K rwdata, 2720K rodata, 1024K init, 252K bss, 19184K reserved, 49152K cma-reserved, 0K highmem)
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    [    0.000000]     vmalloc : 0xe0800000 - 0xff800000   ( 496 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0x(ptrval) - 0x(ptrval)   (10208 kB)
    [    0.000000]       .init : 0x(ptrval) - 0x(ptrval)   (1024 kB)
    [    0.000000]       .data : 0x(ptrval) - 0x(ptrval)   ( 308 kB)
    [    0.000000]        .bss : 0x(ptrval) - 0x(ptrval)   ( 253 kB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] 	Tasks RCU enabled.
    [    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
    [    0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts
    [    0.000000] OMAP clockevent source: timer2 at 24000000 Hz
    [    0.000016] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
    [    0.008074] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
    [    0.017550] OMAP clocksource: timer1 at 24000000 Hz
    [    0.022709] timer_probe: no matching timers found
    [    0.027773] Console: colour dummy device 80x30
    [    0.032355] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
    [    0.039077] This ensures that you still see kernel messages. Please
    [    0.045520] update your kernel commandline.
    [    0.049857] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
    [    0.090037] pid_max: default: 32768 minimum: 301
    [    0.094960] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.101761] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.109763] CPU: Testing write buffer coherency: ok
    [    0.114864] CPU0: Spectre v2: using BPIALL workaround
    [    0.120862] Setting up static identity map for 0x80100000 - 0x80100060
    [    0.127752] rcu: Hierarchical SRCU implementation.
    [    0.132979] EFI services will not be available.
    [    0.138900] devtmpfs: initialized
    [    0.149655] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    [    0.157972] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    [    0.168134] futex hash table entries: 256 (order: -1, 3072 bytes)
    [    0.177806] pinctrl core: initialized pinctrl subsystem
    [    0.183984] DMI not present or invalid.
    [    0.188330] NET: Registered protocol family 16
    [    0.195087] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.225785] l4_wkup_cm:clk:0010:0: failed to disable
    [    0.271336] cpuidle: using governor ladder
    [    0.275625] cpuidle: using governor menu
    [    0.284354] OMAP GPIO hardware version 0.1
    [    0.297244] No ATAGs?
    [    0.297256] hw-breakpoint: debug architecture 0x4 unsupported.
    [    0.318524] edma 49000000.edma: TI EDMA DMA engine driver
    [    0.327074] SCSI subsystem initialized
    [    0.331362] media: Linux media interface: v0.10
    [    0.336204] videodev: Linux video capture interface: v2.00
    [    0.341931] pps_core: LinuxPPS API ver. 1 registered
    [    0.347133] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.356562] PTP clock support registered
    [    0.360614] EDAC MC: Ver: 3.0.0
    [    0.364860] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
    [    0.371681] Advanced Linux Sound Architecture Driver Initialized.
    [    0.379133] clocksource: Switched to clocksource timer1
    [    0.392223] NET: Registered protocol family 2
    [    0.397469] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes)
    [    0.405487] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
    [    0.412805] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
    [    0.419487] TCP: Hash tables configured (established 4096 bind 4096)
    [    0.426123] UDP hash table entries: 256 (order: 0, 4096 bytes)
    [    0.432151] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    [    0.438728] NET: Registered protocol family 1
    [    0.443773] RPC: Registered named UNIX socket transport module.
    [    0.449946] RPC: Registered udp transport module.
    [    0.454776] RPC: Registered tcp transport module.
    [    0.459619] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.467122] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
    [    0.476726] Initialise system trusted keyrings
    [    0.481624] workingset: timestamp_bits=14 max_order=17 bucket_order=3
    [    0.492691] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.499495] NFS: Registering the id_resolver key type
    [    0.504722] Key type id_resolver registered
    [    0.509017] Key type id_legacy registered
    [    0.513283] ntfs: driver 2.1.32 [Flags: R/O].
    [    0.520027] Key type asymmetric registered
    [    0.524246] Asymmetric key parser 'x509' registered
    [    0.529414] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
    [    0.537017] io scheduler noop registered
    [    0.541120] io scheduler deadline registered
    [    0.545745] io scheduler cfq registered (default)
    [    0.550715] io scheduler mq-deadline registered
    [    0.555369] io scheduler kyber registered
    [    0.561186] pinctrl-single 44e10800.pinmux: 142 pins, size 568
    [    0.613573] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
    [    0.623778] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250
    [    0.632954] console [ttyS0] enabled
    [    0.632954] console [ttyS0] enabled
    [    0.640087] bootconsole [omap8250] disabled
    [    0.640087] bootconsole [omap8250] disabled
    [    0.650539] omap_rng 48310000.rng: Random Number Generator ver. 20
    [    0.659324] random: fast init done
    [    0.662995] random: crng init done
    [    0.676323] brd: module loaded
    [    0.685821] loop: module loaded
    [    0.691554] libphy: Fixed MDIO Bus: probed
    [    0.769216] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
    [    0.776918] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
    [    0.784246] libphy: 4a101000.mdio: probed
    [    0.788289] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
    [    0.798382] cpsw 4a100000.ethernet: Detected MACID = 94:a9:a8:88:fe:44
    [    0.805206] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
    [    0.811684] cpsw 4a100000.ethernet: ALE Table size 1024
    [    0.816964] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
    [    0.825520] i2c /dev entries driver
    [    0.830962] cpuidle: enable-method property 'ti,am3352' found operations
    [    0.838069] sdhci: Secure Digital Host Controller Interface driver
    [    0.844404] sdhci: Copyright(c) Pierre Ossman
    [    0.849536] omap_gpio 44e07000.gpio: Could not set line 6 debounce to 200000 microseconds (-22)
    [    0.858277] omap_hsmmc 48060000.mmc: Got CD GPIO
    [    0.863438] omap_hsmmc 48060000.mmc: Linked as a consumer to regulator.1
    [    0.897009] omap_hsmmc 481d8000.mmc: Linked as a consumer to regulator.1
    [    0.929527] sdhci-pltfm: SDHCI platform and OF driver helper
    [    0.937172] ledtrig-cpu: registered to indicate activity on CPUs
    [    0.945689] mmc0: host does not support reading read-only switch, assuming write-enable
    [    0.956866] NET: Registered protocol family 10
    [    0.963061] Segment Routing with IPv6
    [    0.966912] mmc0: new high speed SDHC card at address 5048
    [    0.972625] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    0.979656] mmcblk0: mmc0:5048 SD32G 29.7 GiB 
    [    0.985717] NET: Registered protocol family 17
    [    0.990820] Key type dns_resolver registered
    [    0.995313]  mmcblk0: p1 p2
    [    0.998734] omap_voltage_late_init: Voltage driver support not added
    [    1.006843] Loading compiled-in X.509 certificates
    [    1.030003] mmc1: new high speed MMC card at address 0001
    [    1.036412] mmcblk1: mmc1:0001 M62704 3.56 GiB 
    [    1.041590] mmcblk1boot0: mmc1:0001 M62704 partition 1 2.00 MiB
    [    1.047996] mmcblk1boot1: mmc1:0001 M62704 partition 2 2.00 MiB
    [    1.054517] mmcblk1rpmb: mmc1:0001 M62704 partition 3 512 KiB, chardev (244:0)
    [    1.064425]  mmcblk1: p1
    [    1.074769] tps65217 0-0024: TPS65217 ID 0xe version 1.2
    [    1.221401] tda998x 0-0070: found TDA19988
    [    1.228202] tilcdc 4830e000.lcdc: bound 0-0070 (ops tda998x_ops)
    [    1.234330] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    1.240987] [drm] No driver support for vblank timestamp query.
    [    1.247253] [drm] Cannot find any crtc or sizes
    [    1.252438] [drm] Initialized tilcdc 1.0.0 20121205 for 4830e000.lcdc on minor 0
    [    1.260086] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
    [    1.267487] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz
    [    1.273808] cpu cpu0: Linked as a consumer to regulator.3
    [    1.279380] cpu cpu0: Dropping the link to regulator.3
    [    1.284888] cpu cpu0: Linked as a consumer to regulator.3
    [    1.291599] hctosys: unable to open rtc device (rtc0)
    [    1.297230] ALSA device list:
    [    1.300409]   No soundcards found.
    [    1.308676] EXT4-fs (mmcblk0p2): mounting ext3 file system using the ext4 subsystem
    [    2.269757] [drm] Cannot find any crtc or sizes
    [    3.914563] EXT4-fs (mmcblk0p2): recovery complete
    [    3.921442] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [    3.929700] VFS: Mounted root (ext3 filesystem) on device 179:2.
    [    3.943979] devtmpfs: mounted
    [    3.948571] Freeing unused kernel memory: 1024K
    [    3.953720] Run /sbin/init as init process
    [    4.279734] systemd[1]: System time before build time, advancing clock.
    [    4.325481] systemd[1]: systemd 239 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
    [    4.347804] systemd[1]: Detected architecture arm.
    
    Welcome to Arago 2019.11!
    
    [    4.403333] systemd[1]: Set hostname to <am335x-evm>.
    [    4.426158] systemd[1]: Initializing machine ID from random generator.
    [    4.728993] systemd[1]: File /lib/systemd/system/systemd-journald.service:36 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
    [    4.746339] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
    [    4.826781] systemd[1]: /lib/systemd/system/gadget-init.service:15: Unknown lvalue 'ExecStopPre' in section 'Service'
    [    5.183003] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    5.220621] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [    5.261946] systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
             Mounting POSIX Message Queue File System...
    [  OK  ] Listening on Process Core Dump Socket.
             Starting Load Kernel Modules...
    [  OK  ] Listening on udev Kernel Socket.
    [  OK  ] Created slice system-serial\x2dgetty.slice.
    [    5.490669] cryptodev: loading out-of-tree module taints kernel.
    [    5.500213] cryptodev: driver 1.9 loaded.
             Mounting Kernel Debug File System...
    [    5.547022] usbcore: registered new interface driver usbfs
    [  OK  ] Created slice User and Session Slice.
    [    5.560353] usbcore: registered new interface driver hub
    [    5.566073] usbcore: registered new device driver usb
             Starting Remount Root and Kernel File Systems...
    [  OK  ] Reached target Swap.
    [    5.602583] usbcore: registered new interface driver ftdi_sio
    [    5.611333] usbserial: USB Serial support registered for FTDI USB Serial Device
    [    5.687031] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
             Mounting Temporary Directory (/tmp)...
    [  OK  ] Created slice system-getty.slice.
             Starting udev Coldplug all Devices...
    [  OK  ] Reached target Remote File Systems.
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [  OK  ] Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Reached target Slices.
    [  OK  ] Started Hardware RNG Entropy Gatherer Daemon.
    [  OK  ] Listening on Journal Socket (/dev/log).
             Starting Journal Service...
    [  OK  ] Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Reached target Paths.
    [  OK  ] Mounted POSIX Message Queue File System.
    [  OK  ] Started Load Kernel Modules.
    [  OK  ] Started Journal Service.
    [  OK  ] Mounted Kernel Debug File System.
    [  OK  ] Started Remount Root and Kernel File Systems.
    [  OK  ] Mounted Temporary Directory (/tmp).
             Starting Rebuild Hardware Database...
             Starting Create System Users...
             Starting Flush Journal to Persistent Storage...
             Mounting Kernel Configuration File System...
             Starting Apply Kernel Variables...
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Started Create System Users.
    [  OK  ] Started Apply Kernel Variables.
    [    6.728172] systemd-journald[85]: Received request to flush runtime journal from PID 1
             Starting Create Static Device Nodes in /dev...
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Started Create Static Device Nodes in /dev.
    [  OK  ] Reached target Local File Systems (Pre).
             Mounting /var/volatile...
    [  OK  ] Reached target Containers.
             Mounting /media/ram...
    [  OK  ] Mounted /var/volatile.
    [  OK  ] Mounted /media/ram.
             Starting Load/Save Random Seed...
    [  OK  ] Reached target Local File Systems.
             Starting Rebuild Journal Catalog...
             Starting Rebuild Dynamic Linker Cache...
             Starting Create Volatile Files and Directories...
    [  OK  ] Started Load/Save Random Seed.
    [  OK  ] Started Rebuild Journal Catalog.
    [  OK  ] Started Create Volatile Files and Directories.
             Starting Network Time Synchronization...
             Starting Update UTMP about System Boot/Shutdown...
             Starting Run pending postinsts...
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Reached target System Time Synchronized.
    [  OK  ] Started udev Coldplug all Devices.
    [  OK  ] Started Rebuild Dynamic Linker Cache.
    [  OK  ] Started Rebuild Hardware Database.
             Starting udev Kernel Device Manager...
             Starting Update is Completed...
    [  OK  ] Started Update is Completed.
    [  OK  ] Started udev Kernel Device Manager.
             Starting Network Service...
    [  OK  ] Started Network Service.
             Starting Wait for Network to be Configured...
             Starting Network Name Resolution...
    [  OK  ] Started Network Name Resolution.
    [  OK  ] Reached target Network.
    [  OK  ] Reached target Host and Network Name Lookups.
    [   15.554880] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
    [   15.629470] omap_rtc 44e3e000.rtc: registered as rtc0
    [  OK  ] Found device /dev/ttyS0.
    [   15.959808] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
    [   16.804755] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
    [   16.863484] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
    [   16.986398] omap-aes 53500000.aes: will run requests pump with realtime priority
    [   17.074768] remoteproc remoteproc0: wkup_m3 is available
    [   17.093531] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.sgx on minor 1
    [   17.402680] remoteproc remoteproc0: powering up wkup_m3
    [   17.430743] PM: Cannot get wkup_m3_ipc handle
    [   17.495203] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 242888
    [   17.603310] remoteproc remoteproc0: remote processor wkup_m3 is now up
    [   17.603339] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
    [   17.937617] asoc-simple-card sound: i2s-hifi <-> 48038000.mcasp mapping ok
    [   18.081987] asoc-simple-card sound: ASoC: no DMI vendor name!
    [   18.186950] PM: bootloader does not support rtc-only!
    [   18.629901] net eth0: initializing cpsw version 1.12 (0)
    [  OK  ] Found device /dev/ttyS3.
    [   18.900588] SMSC LAN8710/LAN8720 4a101000.mdio:00: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
    [   19.126214] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [   24.571258] am335x-phy-driver 47401300.usb-phy: 47401300.usb-phy supply vcc not found, using dummy regulator
    [*     ] (1 of 4) A start job is running for…-mmcblk0p1.device (19s / 1min 30s)[   24.680848] am335x-phy-driver 47401300.usb-phy: Linked as a consumer to regulator.0
    [   24.760211] am335x-phy-driver 47401b00.usb-phy: 47401b00.usb-phy supply vcc not found, using dummy regulator
    [   24.872824] am335x-phy-driver 47401b00.usb-phy: Linked as a consumer to regulator.0
    [   24.964681] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
    [   25.036970] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
    [   25.104057] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
    [   25.162004] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [   25.236600] usb usb1: Product: MUSB HDRC host driver
    [**    ] (1 of 4) A start job is running for…-mmcblk0p1.device (20s / 1min 30s)[   25.305628] usb usb1: Manufacturer: Linux 4.19.94-gbe5389fd85 musb-hcd
    [   25.361763] remoteproc remoteproc1: 4a334000.pru is available
    [   25.367668] pru-rproc 4a334000.pru: PRU rproc node pru@4a334000 probed successfully
    [   25.409897] usb usb1: SerialNumber: musb-hdrc.1
    [   25.463024] hub 1-0:1.0: USB hub found
    [   25.490740] hub 1-0:1.0: 1 port detected
    [   25.518444] remoteproc remoteproc2: 4a338000.pru is available
    [   25.529444] pru-rproc 4a338000.pru: PRU rproc node pru@4a338000 probed successfully
    [  OK  ] Found device /dev/mmcblk0p1.
    [  OK  ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
    [  OK  ] Created slice system-systemd\x2dfsck.slice.
             Starting File System Check on /dev/mmcblk0p1...
    [  OK  ] Started File System Check on /dev/mmcblk0p1.
             Mounting /run/media/mmcblk0p1...
    [  OK  ] Mounted /run/media/mmcblk0p1.
    [  OK  ] Started Run pending postinsts.
    [  OK  ] Reached target System Initialization.
             Starting Reboot and dump vmcore via kexec...
    [  OK  ] Listening on RPCbind Server Activation Socket.
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Listening on dropbear.socket.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Started Daily rotation of log files.
    [  OK  ] Reached target Timers.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
    [  OK  ] Reached target Sockets.
    [  OK  ] Reached target Basic System.
             Starting Lightning Fast Webserver With Light System Requirements...
             Starting rc.pvr.service...
             Starting Simple Network Management Protocol (SNMP) Daemon....
    [  OK  ] Started Redis In-Memory Data Store.
    [   36.901774] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ]
             Starting RPC Bind Service...
             Starting Enable and configure wl18xx bluetooth stack...
    [  OK  ] Started Periodic Command Scheduler.
             Starting Save/Restore Sound Card State...
             Starting Print notice about GPLv3 packages...
    [  OK  ] Started D-Bus System Message Bus.
    [  OK  ] Started Job spooling tools.
             Starting Permit User Sessions...
             Starting Start USB gadget...
             Starting Avahi mDNS/DNS-SD Stack...
             Starting Login Service...
    [  OK  ] Started Reboot and dump vmcore via kexec.
    [  OK  ] Started Lightning Fast Webserver With Light System Requirements.
    [  OK  ] Started rc.pvr.service.
    [  OK  ] Started RPC Bind Service.
    [  OK  ] Started Enable and configure wl18xx bluetooth stack.
    [  OK  ] Started Save/Restore Sound Card State.
    [  OK  ] Started Permit User Sessions.
    [  OK  ] Started Serial Getty on ttyS3.
    [  OK  ] Started Serial Getty on ttyS0.
    [   38.240606] using random self ethernet address
    [  OK  ] Started Getty on tty1.
    [   38.257051] using random host ethernet address
    [  OK  ] Reached target Sound Card.
    [   38.286023] using host ethernet address: 94:A9:A8:88:FE:46
    [   38.286090] using random self ethernet address
    [  OK  ] Started NFS status monitor for NFSv2/3 locking..
    [   38.309524] using random host ethernet address
             Starting weston.service...
    [   38.314056] using host ethernet address: 94:A9:A8:88:FE:46
    [   38.369424] usb0: HOST MAC 94:a9:a8:88:fe:46
    [  OK  ] Started Login Service.
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [   38.471436] usb0: MAC f2:64:83:1f:f4:5a
    [  OK  ] Started Simple Network Management Protocol (SNMP) Daemon..
    [   38.581155] Mass Storage Function, version: 2009/09/11
    [   38.586342] LUN: removable file: (no medium)
    [   38.651193] LUN: removable read only file: /dev/mmcblk0p1
    [   38.656637] Number of LUNs=1
    [  OK  ] Found device /dev/ttyGS0.
    [   38.742392] g_multi gadget: Multifunction Composite Gadget
    [   38.747931] g_multi gadget: g_multi ready
    [   38.872985] IPv6: ADDRCONF(NETDEV_UP): usb0: link is not ready
    [   39.196532] g_multi gadget: high-speed config #2: Multifunction with CDC ECM
    [   39.205668] IPv6: ADDRCONF(NETDEV_CHANGE): usb0: link becomes ready
    [  OK  ] Started Start USB gadget.
    [  OK  ] Started Serial Getty on ttyGS0.
    [  OK  ] Reached target Login Prompts.
             Starting Synchronize System and HW clocks...
    [  OK  ] Started Synchronize System and HW clocks.
    [  OK  ] Started weston.service.
             Starting Matrix GUI...
             Starting telnetd.service...
    [  OK  ] Started Matrix GUI.
    [  OK  ] Started telnetd.service.
             Starting busybox-udhcpd.service...
             Starting thttpd.service...
    [  OK  ] Started busybox-udhcpd.service.
    [  OK  ] Started thttpd.service.
    ***************************************************************
    ***************************************************************
    NOTICE: This file system contains the following GPLv3 packages:
    	autoconf
    	bash-dev
    	bash
    	bc
    	binutils
    	cifs-utils
    	cpio
    	cpp-symlinks
    	cpp
    	dosfstools
    	elfutils
    	findutils
    	g++-symlinks
    	g++
    	gawk
    	gcc-symlinks
    	gcc
    	gdb
    	gdbserver
    	gettext
    	glmark2
    	gstreamer1.0-libav
    	gzip
    	hidapi
    	libbfd
    	libcairo-perf-utils
    	libdw1
    	libelf1
    	libgdbm-compat4
    	libgdbm-dev
    	libgdbm6
    	libgettextlib
    	libgettextsrc
    	libgmp10
    	libidn2-0
    	libmavconn
    	libmpc3
    	libmpfr6
    	libreadline-dev
    	libreadline7
    	libunistring2
    	m4-dev
    	m4
    	make
    	mavlink
    	mavros-extras
    	mavros-msgs
    	mavros
    	nettle
    	pdm-anomaly-detection
    	socketcan-interface
    	swig-dev
    	swig
    	which
    
    If you do not wish to distribute GPLv3 components please remove
    the above packages prior to distribution.  This can be done using
    the opkg remove command.  i.e.:
        opkg remove <package>
    Where <package> is the name printed in the list above
    
    NOTE: If the package is a dependency of another package you
          will be notified of the dependent packages.  You should
          use the --force-removal-of-dependent-packages option to
          also remove the dependent packages as well
    ***************************************************************
    ***************************************************************
    
     _____                    _____           _         _   
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
                  |___|                    |___|            
    
    Arago Project http://arago-project.org am335x-evm ttyS0
    
    Arago 2019.11 am335x-evm ttyS0
    
    am335x-evm login: root
    root@am335x-evm:~# uname -a
    Linux am335x-evm 4.19.94-gbe5389fd85 #1 PREEMPT Sun Apr 19 03:43:09 UTC 2020 armv7l GNU/Linux
    root@am335x-evm:~# 
    
    

    Regards,
    Vinu

  • Thanks for the details.

    I'll download SDK 6.

    Some Questions:

    1. Did you build the u-boot2025.01 from scratch?

        Or did you use the sdk11 prebuilt u-boot2025.01?

    2. To build u-boot2025.01 from scratch, which files need to be patched?

         I assume 'am335x_evl-defconfig' is the correct defconfig file to use from u-boot2025.01 project?

  • Hi Bob,

    1. I've used the prebuilt U-boot.

    2. No need to patch anything. If you are using a custom board, update the DTS and config files.

    am335x_evm_defconfig is the default config file, which can be used as the reference.

    For building U-boot, please refer 

    1. https://software-dl.ti.com/processor-sdk-linux/esd/AM335X/11_02_05_02/exports/docs/linux/Foundational_Components/U-Boot/BG-Setup-OMAP.html
    2. https://software-dl.ti.com/processor-sdk-linux/esd/AM335X/11_02_05_02/exports/docs/linux/Foundational_Components/U-Boot/BG-Build-OMAP.html

    Regards,
    Vinu

  • Hi  ,

    Please let me know why you've rejected the answer.

    Did any of the above mentioned steps not work for you?

    Regards,
    Vinu

  • Closing the thread, as it is stale.

    Regards,
    Vinu