This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0-SDK: MCAL_MSPM0_01.00.00.00 gmake build error 2

Part Number: MSPM0-SDK

I have some difficulties with MCAL 1.0.0 package build from gmake, please find the screenshot attached.3889f27b-c155-47b2-b2c3-ef42f06beac5.png The MCAL package is downloaded straight from the portal, and unzipped before gmake build command. The command was: gmake -s can_app PLATFORM=MSPM0G351x PROFILE=debug COMPILER=IAR. 

Thank you for helping out.

Best regards,

Csaba

  • Hi Csaba,

    From the looks, it seems that Can.oem0plus is not in the folder. Can you double check if the file is located in the location mentioned?

    An alternative, it could be to store the MCAL package into a single MCAL folder instead of 2 (i.e. why is there two folders with the same name?)

    Best Regards,

    Diego Abad