Other Parts Discussed in Thread: TMS570LS20216
Hi,
We are using TMS570LS20216 processor (144pin package). As per thr TRM, MIBSPI5 can be configured as parallel mode.
But as per our requirement we don not need it it operate in Parallel mode. I have read two registers which mention about configuring in Normal SPI mode for this module.
Is it possible to configure this module working as same as SPI1 and SPI3 ?
For the 144pin package, we can operate the SPI5 in 2pin parallel mode if we want. If i configure this as normal SPI mode, what are the default pins that will be used for communication ? Suppose if MISO0 is used as SPI function in this module, will the other pin MISO2 can be used as GPIO ?
Thanks in advance.