Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28P65X: Customer Reported Issue – TMDSCNCD28P65X – Request for Defect Confirmation

Part Number: TMDSCNCD28P65X

Dear TI Team,

A customer has reported an issue with TMDSCNCD28P65X. The part is displaying an error and is not functioning properly.

Issue Details:

  • Number of defective units: 1
  • Is the error occurring immediately or after some time of operation?
    The error occurs immediately.
  • Is the XDS110 debugger detected correctly in Device Manager?
    Yes, the XDS110 is detected correctly in Device Manager.
  • Have you tried this controlCARD on a known-good baseboard or tested another board on the same setup?
    The customer has tested the TI controlCARD.
  • Are the 3.3V and 1.2V rails stable, and is the RESET signal not held low?
    The customer confirmed that the 3.3V rail is stable but is unsure how to verify the RESET signal.

For your reference, the relevant images are attached.

Could you please review the information and confirm whether the part is defective?
WhatsApp Image 2026-06-25 at 13.29.09 (1) (1) (1).jpegWhatsApp Image 2026-06-25 at 13.29.09 (1) (2).jpegimage (31) (1).png