This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2612: Drive strength for PSRAM

Part Number: AM2612

Hello team,

what is the default driver strength for AM261 when connected to PSRAM?
Is this set to 50 Ohm?

Does the PHY tuning algorithm adjust to this?

Best regards
Manuel

 

  • PHY tuning algo doesn't compensate for drive strength and drive strength is a parameter in flash/psram config space, controller will only send a control command to set the drive strength to a required value. So you can basically use application to set the same.