This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM69A: The QSGMII issue for AM69A

Part Number: AM69A

Hi,

AM69A uses the Serdes2 TX3 and RX3 lanes to perform QSGMII Ethernet function with YT8614. 

After configuring from the reference settings, it cannot access the internet.

The YT8614 driver is provided by the original chip manufacturer and can be read from MDIO to YT8614 normally.

There is also a link response on the differential Ethernet cable, but it cannot ping the network.

I want to confirm whether the configuration of AM69A is correct. 

The below is our QSGMII configuration:

qsgmii configuration.txt