Other Parts Discussed in Thread: LMFLASHPROGRAMMER
Hello,
I've been working with an LM4F232H5QD eval board to evaluate this family for a new design. I can program the MCU reliably using a standard ICDI board (BD-ICDI-B) connected to the JTAG port. However, the programming performance is erratic if I try to use the built-in ICDI function of the eval board.
I'm using the latest version of LM Flash Programmer (build 1381), and have tried 32-bit XP as well as 64-bit Win 7 on two separate PCs with the same results. I've been using the precompiled qs-logger app binary for the board, and the eval board is totally stock.
The problem is that the programming or verify process in LM Flash Programmer will error out before completion, and in a somewhat random fashion.
I've done a lot of searching, and haven't found anything directly pertinent to this issue. I did find a reference to the new ICDI Firmware Update function in LM Flash Programmer, and updated the firmware, but that has not totally solved the issue. It seems to program more consistently, but still usually fails to verify.
Any ideas?
Thanks,
---Karl