Part Number: MSPM33C321A
I am using the SPI to send a bit stream. I found that the Motorola SPI mode leaves gaps between the bytes. The TI Synchronoud mode does not, but it puts an extra bit into the first byte.
I made a slight modification to the "spi_controller_multibyte_fifo_poll_LP_MSPM33C321A_nortos_ticlang" example to show the problem.
#include "ti_msp_dl_config.h"
/*
* Number of bytes for SPI packet size
* The packet will be transmitted by the SPI controller.
* This example uses FIFOs with polling, and the maximum FIFO size is 4.
* Refer to interrupt examples to handle larger packets.
*/
#define SPI_PACKET_SIZE (2)
/* Data for SPI to transmit */
// packet size 4
//uint8_t gExpectedRxPacket[SPI_PACKET_SIZE] = {0x1, 0x2, 0x3, 0x4};
//uint8_t gTxPacket[SPI_PACKET_SIZE] = {0xAA, 0x00, 0xFF, 0x55};
// packet size 2
uint8_t gExpectedRxPacket[SPI_PACKET_SIZE] = {0x1, 0x2};
uint8_t gTxPacket[SPI_PACKET_SIZE] = {0xAA, 0x55};
volatile uint8_t gRxPacket[SPI_PACKET_SIZE];
#ifdef __SLATE_INTERNAL__
volatile bool gTransactionCompleted = false;
#endif
int main(void)
{
SYSCFG_DL_init();
#ifdef __SLATE_INTERNAL__
__BKPT(0);
#endif
/* Fill TX FIFO with data and transmit to SPI Peripheral */
DL_SPI_fillTXFIFO8(SPI_0_INST, &gTxPacket[0], SPI_PACKET_SIZE);
/* Wait until all bytes have been transmitted and the TX FIFO is empty */
while (DL_SPI_isBusy(SPI_0_INST))
;
for (uint8_t i = 0; i < SPI_PACKET_SIZE; i++) {
gRxPacket[i] = DL_SPI_receiveDataBlocking8(SPI_0_INST);
}
#ifdef __SLATE_INTERNAL__
gTransactionCompleted = true;
#endif
/*
* If this example is used with the spi_peripheral_multibyte_fifo_poll
* example, the expected data to receive in gRxPacket is
* {0x01, 0x02, 0x03, 0x04}.
*/
/* If write and read were successful, toggle LED */
while (!DL_SPI_isTXFIFOEmpty(SPI_0_INST))
;
int allCorrect = 1;
for (int i = 0; i < SPI_PACKET_SIZE; i++) {
if (gExpectedRxPacket[i] != gRxPacket[i]) allCorrect = 0;
}
if (allCorrect == 1) {
DL_GPIO_setPins(GPIO_LEDS_PORT, GPIO_LEDS_PASS_LED_PIN);
}
else{
DL_GPIO_setPins(GPIO_LEDS_PORT, GPIO_LEDS_FAIL_LED_PIN);
}
__BKPT(0);
}
The only real difference is to change the data being sent and changing the SPI mode.
When using the example's Motorola 4 wire SPI mode, I get this:

You can count that there is a gap between bytes and 16 clocks. When I switch to the TI Synchronous:

The gaps are gone, but now I get 17 clocks. On some of my tests, it actually stretches the first pulse so I get two ones in a row where there should be only one.
I did not see any errata that pertained to this. Am I doing something wrong?