Part Number: AM2612
Other Parts Discussed in Thread: UNIFLASH
Dear TI Support Team,
I have,
AM261-LP,
ind_comms_sdk_am261x_2025_00_00_08
I am using the TI UniFlash tool to program a device through a JTAG session, and I would appreciate clarification regarding the load address used for the .mcelf_xip image.
I noticed that the .mcelf_xip file is programmed using the address 0xE0000000. Could you please confirm whether this is an actual memory-mapped address in the device, or whether it is only a recognized/metadata address used by UniFlash to identify the image as an XIP file?
In the Profinet_device_demo example, the linker.cmd file defines the flash region as:
This suggests that 0x60100000 is the execute-in-place (XIP) memory region. If that is the actual XIP execution address, why is the .mcelf_xip image flashed at 0xE0000000 instead?
Could you please explain the relationship between these two addresses and confirm the recommended UniFlash programming address for the .mcelf_xip image?
Thank you for your support.
Best Regards,
Parag Vora